There N6781A source measure unit plugs into the N6705B and is a high resolution device with a seamless ranging feature that provides a 28-bit dynamic range. Most oscilloscope have an 8-bit resolution that cannot measure very small signals in the presence of large signals. For an overview, watch the video on Current Probe w/ Oscilloscope Compared to Seamless Current Measurement on N6781A Source.
Applies to: N6781A, N6782A, N6784A, N6785A, N6786A
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |